Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use new Easergy Studio to download current settings and import the same settings instead of S1 Studio in Easergy P63x relay ?
Yes ,it is possible to download setting from old device & import to new devise using Easergy studio.

First you need to convert the setting file for the new model (Right click on the setting file then click covert setting file) & please save the same in your local system.

After convert the setting file ,you can add the setting file from Right click of the setting file then click add existing file.