Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we offer mounting hardware for the ATV630 drives?
Issue:
Altivar Process drives mounting hardware.

Product line:
Altivar Machines, Altivar Process Drives

Environment:
All models and serial numbers

Cause:
Customer is asking for a parts kit to wall mount the Altivar 630 Process Drive.  There are no parts kits listed in the manuals.

Resolution:
For the wall mounted drives, we do not offer a parts kit to install.  We provide the mounting hole sizes in the Installation manual for reference.

See attached for the sizes.

Schneider Electric Nigeria

Attachment(s)
ATV6xx mounting holes.JPG.jpg [58.35 KB]