Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What functions can be assigned to an ATV212 logic input?
Issue:
Trying to assign functions to an ATV212 logic input.

Product Line:
ATV212

Environment:
All models

Cause:
Explore VFD control options

Resolution:
The ATV212 has assignable logic input terminals F / R / RES / VIA.
Please see the attached file for all Logic Input Functions

Schneider Electric Nigeria

Attachment(s)
ATV212 Logic Input Functions.pdf [1.93 MB]