Issue:
External keypad on the ATV340.
Product Line:
Altivar 340
Environment:
All
Cause:
Part number request
Resolution:
Yes, the ATV340 works with the VW3A1113 external keypad. This remote keypad is not shipped with the ATV340. It must be ordered separately.
https://www.se.com/us/en/product/VW3A1113/plain-text-display-terminal---128-x-64-pixels---ip21/

External keypad on the ATV340.
Product Line:
Altivar 340
Environment:
All
Cause:
Part number request
Resolution:
Yes, the ATV340 works with the VW3A1113 external keypad. This remote keypad is not shipped with the ATV340. It must be ordered separately.
https://www.se.com/us/en/product/VW3A1113/plain-text-display-terminal---128-x-64-pixels---ip21/
Released for: Schneider Electric Nigeria