Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Altivar Process ATV630 drives, Booster function configuration with multidrive architecture.
Example with booster control , multidrive configuration (with master redundancy) using 3 drives, all equipped by VW3A3721 card.

List of parameters that must be configured at first:
- Motor data + autotuning
- Basic setting (ACC, DEC, LSP, HSP)
- Macro configuration = booster control

Then the rest of parameters in the example are tailored for:
- pressure control (feedback on AI2, but can be used different input, pressure sensor with 0-10bars, internal setpoint 3.5bars, scaling PIF1, PIF2, PAL, PAH, PIP1, PIP2 can be modified)
- distributed mode (MPST)
- stage/de-stage conditions and method based on feedback (possible to change it to speed)
- first drive is master (MPDT=master). For second and third drive necessary to configure MPDT="master or slave"

Configuration for second and third drive will be the same except:
Second drive must have MGID=2, third drive must have MGID=3
Drives must have different IP address (VW3A3721)

Regarding the wiring:
1. All drives must have signal (application pressure) on their analog input. AI2 in this example. if signal from pressure sensor cannot be distributed to all 3 drives, external signal splitter must be added.
2. Ethernet cable wired for all drives (on VW3A3721, not embedded eth port). It is possible to wire them as daisy chain (Drive1.VW3A3721 - Drive2.VW3A3721.LeftRJ45, Drive2.VW3A3721.rightRJ45 - Drive3.VW3A3721) but then in case of power down on drive 2, the drive1 and 3 cannot work. Better to use simple switch and wire all 3 drives into switch.
3. All 3 drives must be in RUN (run command present). The best if RUN command is first applied on slaves, then on master.

Schneider Electric Nigeria

Attachment(s)
Booster.psx [308.74 KB]