Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the NFPA Hazard Rating for Smart-UPS?


Issue:

What is the NFPA Hazard Rating for Smart-UPS?

Product Line:

Smart-UPS

Environment:

All models, All Serial Numbers

Cause:

"NFPA 704: Standard System for the Identification of the Hazards of Materials for Emergency Response" is a standard maintained by the U.S.-based National Fire Protection Association. Some local jurisdictions require this information for all installed equipment

Resolution:

The NFPA Hazard Rating for non-spillable lead acid batteries is based on Sulfuric acid:

Flammability (Red) = 0
Health (Blue) = 3
Reactivity (Yellow) = 2  (Sulfuric acid is water-reactive if concentrated)


img1

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings