Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 74 - Trip/closing circuit supervision?
To detect trip circuit and closing circuit failures, Sepam monitors:
  • shunt trip coil connection
  • closing coil connection
  • matching of breaking device open/closed position contacts
  • execution of breaking device open and close orders.
The trip and closing circuits are only supervised when connected as shown in attached photo.

Schneider Electric Nigeria

Attachment(s)
ANSI 74.PNG.png [100.61 KB]