Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to generate a PTO (pulse train output) using a M241 controller with SoMachine?

Issue:
This is a step by step procedure on how to write a small program in SoMachine to generate a PTO (pulse train output) using a M241 controller

Product Line:
M241 controllers

Environment:
SoMachine v4.3

Cause:
To have a starting project that will help a customer generate a PTO (pulse train output) with a M241 controller

Resolution
1. Start a new project in SoMachine and select a M241 controller
2. Go to the Logic Builer. Go to View / Classic Navigators / Devices. This will open a window called Devices.
3. In the Devices window double-click on Pulse_Generators. This will open a window called Pulse_Generators.
4. In the Pulse_Generators window select a Pulse generation function by clicking on the Value field. Select PTO and hit Enter
5. Select the Output Mode. You have four options. For this resolution we will select Quadrature
6. Select the outputs to be used by selecting a Fast output in the "A output location" and "B output location"
7. The Instance Name is the name that will be used by the input pin "Axis" of the MC_xx_PTO function blocks. You can leave the default PTO_0 or change it
8. Create a POU and add it to the Mast task. To create a POU go to Devices window / right click on Application / Add object / POU. Select  CFC for this example, any other implementation language can be used. To add the POU to the MAST task just drag it there
9. Double-click on the new POU. From the Toolbox window select "Box" and then click in the POU window.
10. We will create the following function blocks: MC_Power_PTO, MC_Stop_PTO, MC_ReadActualPosition_PTO, MC_MoveRelative_PTO, MC_MoveVelocity_PTO. Other function blocks can be used
11. For the Axis pin we will type in PTO_0 or if you change the Instance name from step 7, used the new name.
12. Build your project and download it to your controller. Tu build it go to Build / Build. To download go to Online / Multiple Download / Always perform a full download. This will update the boot application and download the project to the RAM. Connect to your controller by going to Online / Login.
13. To enable MC_Power_PTO function block, pin Enable and DriveReady have to be TRUE. You can create variables that you can turn ON or you can type the word TRUE instead of a variable
14. We can generate an unlimited pulse train output with a fixed frequency by using the MC_MoveVelocity_PTO. You will need to have values entered at least for Velocity, Acceleration, Deceleration and Direction
14. By turning the Execute bit ON of the MC_MoveVelocity_PTO function block, the M241 will generate a PTO with a frequency equal with the Velocity value.
15. To stop the pulses execute a MC_Stop_PTO
16. You can generate a finite number of pulses by executing the MC_MoveRelative_PTO. You will have to have values entered at least for Distance, Velocity, Acceleration, Deceleration. After that you will have to turn the Execute bit ON.



This completes the step by step procedure on how to write a small program in SoMachine to generate a PTO (pulse train output) using a M241 controller

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)