How can we help you today?

Why is the text on my SBP3000 upside down?

Product Line: SBP3000

Cause: The artwork is correct. The SBP3000 is intended to be wall mounted or used in tower format.

Resolution: The SBP3000 can be rack mounted but it will have the artwork text upside down, unless the bypass panel is oriented with the AC input on the right and switch on the left.

Schneider Electric Nigeria

Attachment(s)
SBP3000.png [29.88 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre