Switches used for load-breaking in SM6 36kV complies to electrical endurance class "E3" to IEC 62271-103,
The switch can break up to 100 breaks at its rated current (Ir) at a power factor of 0.7.
The switch can break up to 100 breaks at its rated current (Ir) at a power factor of 0.7.
Released for: Schneider Electric Nigeria