Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 87M - Machine differential?
Phase-to-phase short-circuit protection, based on phase by phase comparison of the
currents on motor and generator windings.
Characteristics
  • instantaneous tripping
  • fixed high set point for fast tripping for violent faults, with no restraint
  • percentage-based characteristic with fixed slope and adjustable low set point
  • tripping restraint according to percentage characteristic activated by detection of:
*external fault or machine starting
*sensor saturation or disconnection
*transformer energizing (harmonic 2 restraint)