Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of ANSI 78PS - Pole slip?
Protection against loss of synchronism on synchronous
machines, based on calculated active power.
2 types of operation:
  • tripping according to the equal-area criterion, time-delayed
  • tripping according to power swing (number of active power swings):

*suitable for generators capable of withstanding high electrical and mechanical constraints

*to be set as a number of rotations.

The 2 types of operation may be used independently or at the same time.