Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the real Starting time of ATS01 , ATS130 Altistart softstarters in relation to the Front Potentiometers settings?

ATS01, ATS130 has very simple logic for limiting starting current and so there are no exact values of starting time. The starting ramps are not fully controlled like in ATS22 or ATS480.
See attached resolution to know the influence of setting on starting current and time. Although it was written for ATS01, it is applicable for ATS130 as well.

Schneider Electric Nigeria

Attachment(s)
Sol075 - ATS01 Start time and Initial voltage setting.pdf [280.15 KB]