Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure ION9000 basic settings using the web interface?

Issue
A user may require configuring ION9000 basic settings using its web interface.

Product line
ION9000

Environment
ION9000

Cause
Users can configure/view ION9000 basic settings using the meter's web interface.

Resolution
Using a browser:

  1. Type in the meter's IP address in the address bar and hit Enter. "https://IP address)
  2. In ION 9000 Login Page type the meter username and password (the default username and password are 9000 and 0, respectively).
  3. Navigate to the Setup tab.
  4. Click on the metering menu.
  5. From here you will be able to navigate to the appropriate menus for Basic and Advanced Settings configuration.


Basic settings menu
1

Advanced Settings menu
2