Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to display several panels of a Vijeo Designer application using in same time several targets and HMIZMDARX Multi Display Adaptor?
Goal:  To display two different panels of a same Vijeo Designer project with panel 1 displayed on the Host HMIG5U2 and panel 2 displayed on the Client through the Webgate.
To test, we’ll use:
- a HMIG5U2 with HMIDT551 as Host and
- a HMIDT551 with HMIZMDARX module as Client.

Please refer to the attached pdf document.

Schneider Electric Nigeria

Attachment(s)
FAQ_Multi display projet.pdf [2.82 MB]