Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the required control voltage for the ATS48?
Issue:
Required control voltage for the ATS48.

Product Line:
Altistart 48 Soft Starter

Environment:
All

Cause:
Installation documentation

Resolution:
ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz
ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz
This is AC voltage, and is applied to the CL1 and CL2 terminals.

Electrical Characteristics

Schneider Electric Nigeria

Attachment(s)
ATS48 wiring.pdf [69.85 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings