Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the MTBF of the BMXFCW303 (FCN 2 x 20 wire 3m cable for Modicon X80)?
Issue
What is the MTBF of the BMXFCW303 (FCN 2 x 20 wire 3m cable for Modicon X80)?

Product Line
Modicon X80 Modules

Resolution
Below are the MBTF values in hours:

MTBF 30°C Continuous: 166,666,666,666
MTBF 30°C Intermittent: 166,666,666,666
MTBF 60°C Continuous: 166,666,666,666
MTBF 60°C Intermittent: 166,666,666,666
MTBF 85°C Continuous: 166,666,666,666
MTBF 85°C Intermittent: 166,666,666,666

Nb Cpt Missing: 0
Nb Cpt Missing * Qty: 0
Nb Cpt Total * Qty: 6
Ratio Nb Cpt Missing / Nb Cpt Total: 0.00%