Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where do I purchase the Lexium Integrated Drive with Reference Part Number ILS2K573S2212?

Issue

Where do I purchase the Lexium Integrated Drive with Reference Part Number ILS2K573S2212?

Product Line

Lexium ILS Integrated Drives

Resolution

The Lexium Integrated Drive with reference number ILS2K573S2212 is a special proprietary model specifically made for an OEM machine builder.

This model is proprietary to the OEM and is not available for purchase directly from Schneider Electric.

Please contact the OEM machine builder of the machine in which this motor is incorporated on to obtain a spare or a replacement.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings