Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Default password is not working in Easergy Micom Px3x relay?

Issue :

Default password is not working in Easergy Micom Px3x relay?

Product family:

Easergy Micom Px3x relays

Resolution:

Starting with firmware version -675 the California Password Law is implemented in MiCOM Px30 devices, therefore usage of default password is no longer possible. All passwords are required to be unique, so the user see prompt for a password change, either before accessing to it with the Easergy Studio tool or from the HMI.

Thanks to refer the document attached for more details .

Please contact our customer care if you need any further support.

Schneider Electric Nigeria

Attachment(s)
TQ_PAST-2023-BW-03-a MiCOM Px30-675 password change (1).pdf [2.21 MB]