Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the ATV630 outdoor drive not to start the motor in auto mode?

Issue:
ATV630 HOA is not starting in auto mode.

Product Line:
ATV630 Outdoor Drive only

Environment:
All

Cause:
Customer supplied auto start contact is open

Resolution:
Close field terminal block 208 and 208