Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
More motors connected to one Variable speed drive in parallel

Article available in these languages: Spanish

Refer to manual of your Drive to identify correct motor control type selection and possible limitation.

In case of motors in parallel VSD can not tell if they are loaded equally. One motor can be underload and other can be overload. To have safe installation thermal protection is required for each motor.