Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the function of ACE850TP and ACE850FO network interfaces?
ACE850 multi-protocol communication interfaces are for Sepam series 40 and Sepam series 80 units.
They have two Ethernet communication ports to connect a Sepam unit to a sing
Ethernet network depending on the topology (star or ring):
  • For a star topology, only one communication port is used.
  • For a ring topology, both Ethernet communication ports are used to provide redundancy. This redundancy conforms to the RSTP 802.1d 2004 standard.
Either port can be used for connection:
  • To the S-LAN (Supervisory Local Area Network) port to connect a Sepam unit to
an Ethernet communication network dedicated to supervision, using either of the following protocols:

1- IEC 61850
2- eModbus TCP/IP TRA 15.
  • To the E-LAN (Engineering Local Area Network) port, reserved for remote parameter setting and operation of a Sepam unit using SFT2841 software.
There are two versions of the ACE850 interface, which are identical except for the type of port featured:
  • ACE850TP (Twisted Pair), for connection to an Ethernet network (S-LAN or
E-LAN) using a copper RJ45 10/100 Base TX Ethernet link.
  • ACE850FO (Fiber Optic), for connection to an Ethernet network (S-LAN or E-LAN)
using a 100Base FX fiber optic connection (star or ring).