Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an InFA or internal error 10 on the ATV630 and ATV930 Process drives?
Issue:
InFA or internal error 10 on the ATV630 and ATV930.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
The external supply voltage is to high.
The P24 voltage input for the customer 24vdc supply is monitored against
overvoltage. The error raise at P24 > 30.5vdc

Resolution:
Check the external 24V supply make sure its less than 30.5vdc