Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EcoStruxure Control Expert 14 returns message Integrity Check - C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK\Srcsdk.dll
Issue
If I open 'EcoStruxure Control Expert' after installing the software, I get a message indicating 'Integrity Check - 'C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK\Srcsdk.dll'
If I click on OK to close the message window, 'Control Expert' starts up.

Product line
EcoStruxure Control Expert 14.

Environment
Windows 8, Windows 10

Resolution
The following steps can be used to resolve the issue:
  1. Navigate to the path described in the 'Integrity check' error window ('C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK).
  2. Locate the file named 'IntegrityCheckSRCSDK.bin'
  3. Delete the file.
  4. If there are multiple files starting with the name IntegrityCheck...bin, delete those as well.
  5. Insert the DVD for Unity and run 'setup.exe'.
  6. If you get an error regarding the installation of 'Microsoft Visual C++ 2012 Update 4 Redistributable...have failed) Do you want to continue with the installation,' click on 'Yes' to proceed.  The reason for the failure message  is due to the  software already being installed on the PC.
  7. Click on 'Next'.
  8. Select 'Repair to repair the installation.
  9. Launch the application after installation repair completes.