Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV630 - Wants to display the modbus run time on the HMI
Issue:
How to read the Modbus "run time" on a HMI for the Altivar Process Drive.

Product Line:
ATV630, ATV930

Environment:
All serial numbers

Cause:
Wants to display the run time on the HMI

Resolution:
Beginning with ATV630 firmware version 2.4IE11 and ATV930 version 2.1IE17 the keypad can display the Run Time in Days, Hours,Minutes and  Seconds.
When reading the Runtime over a network the value will be in seconds
rtH Parameter name: Total motor operating time Terminal display: [Run time]
Logic address: 3244 = 16#0CAC (unsigned 32 bit)

Previous versions only displayed the run time  in seconds.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings