Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the polarity of A and B Terminals when using BACnet on ATV212 drive?
Issue:
Polarity of A and B Terminals when using ATV212 BACnet.

Product Line:
ATV212, Altivar 212

Environment:
All

Cause:
NA

Resolution:
Terminal B is positive(+) and terminal A is negative(-).