Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What versions of Vijeo Designer are supported for SoMachine v4.x?

Issue
What versions of Vijeo Designer are supported for SoMachine v4.0, v4.1,v 4.2 and v4.3?

Product Line
SoMachine, Vijeo Designer

Environment
Configuration software on Windows PC

Resolution
See the table below for supported Vijeo Designer versions on SoMachine v4.0 and above:

SoMachine VersionVijeo Designer version that is included with version of SoMachineVijeo Designer Service Pack released SoMachine that can be installed on top:Additional Compatible Service Packs intended for Standalone Vijeo Designer that work for SoMachine:
v4.0v6.1 SP4
v4.1v6.2
v4.1 SP1v6.2 SP2v6.2 SP5 to SP8
v4.2v6.2 SP4.1v6.2 SP5.1v6.2 SP6 to SP8
v4.3v6.2 SP4.1v6.2 SP6.1v6.2 SP7 to SP8
v4.3 Patch 2v6.2 SP4.1v6.2 SP6.1v6.2 SP7 to SP8


If you have SoMachine v4.2 or v4.3, the Vijeo Designer Service Packs can be found in the Schneider Electric Software Update Tool launched from the Windows Start -> Programs -> Schneider Electric -> Software Update -> Software Update (shortcut icon)"

NOTE:
HMISCU new from the factory manufactured late 2023 or newer with SV8.0 written on the sticker on the back require Vijeo Designer v6.2 Service Pack 8 Hotfix 22.
Please contact tech support for the installation files.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)