Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default IP address of a Premium PLC or ETY Ethernet module?

Article available in these languages: Japanese

Issue:
Default IP address of a Premium PLC or ETY Ethernet module


Product Line:
Premium PLC


Resolution:
The ETY port on the processor or ETY module has a default IP address which is derived from the last 2 octets of the MAC address. The first 2 octets are fixed at 85.16.x.x ;  where x.x is the last 2 octets of the MAC address. For example, If the MAC address is 00.80.F4.02.EA.6A then the IP address will be 85.16.234.106
EA Hex = 234 Decimal
6A Hex = 106 Decimal

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings