Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the BMXDAI1614 as a traditional input module if I disable the "Wiring Check" option?
Yes. The BMXDAI1614 will operate as a traditional input when the "Wiring Check" option is turned off.

With this module, you have the ability to monitor each channel separately to determine if a sensor is connected. It does this by monitoring the leakage current of the sensor when it is off. If it detects that no sensor is connected, it will set bit 9 of the CH_FLT.

100766_IMG

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings