Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I assign a second Run forward command to Altivar Process drives?
Issue:
Assign a second Run Forward command to Altivar Process Drives Logic input.

Product Line:
Altivar Drives, ATV600, ATV900

Environment:
All

Cause:
Want to install a separate remote external +24vdc start/stop command to DI3

Resolution:
No, You can not assign 2 "Run Forward" commands to different logic/digital inputs.