Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Vario switch be extended by an Auxiliary contact in ATV650D30N4?
Yes, it is possible.
ATV650, size B (30kW-45kW) has free space on the sides (42mm on left side and more than 100mm on right side).
This ATV size has Vario V5 inside, use aux. block compatible with V5 body.

Schneider Electric Nigeria

Attachment(s)
Vario V5.jpg [58.18 KB]