Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find instructions on wiring the ZBRA1 Relay antenna?
Issue:
Wants to confirm the wiring and installation of the ZBRA1, wireless relay antenna.

Product line:
Push Buttons and Operator Interface

Environment:
XB5 Wireless pushbuttons

Cause:
Wiring confirmation, polarity for control wires

Resolution:
See the attached installation instructions for the ZBRA1 relay antenna.

The Blue wire is for Neutral or 0V
The Brown wire is the hot wire for 24...240VAC/DC

Schneider Electric Nigeria

Attachment(s)
ZBRA1 instr S1A57194_05.pdf [894.33 KB]