Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What causes EtHF [Embd Eth Com Interrupt] on the ATV340 series drives and how do I correct it?
Issue:
Why is the ATV340 tripping on [EtHF] Embedded Ethernet Communication Interrupt fault?

Product Line:
ATV340

Environment:
ATV340 series drive controlling via Embedded Ethernet

Cause:
Communication interruption on the Ethernet IP or Modbus TCP bus

Resolution:
 Check the communication connections and cables
 Try a different Ethernet Cable
 Try a different Port on the switch or gateway
 Refer to the Ethernet user manual.