Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
On the PowerTag A9 F63 model, ref. A9MEM1562 if I try to be consistent with the flat cable position, the LED of the module is upwards. Should I twist the flat cable to have the LED down?
This has no impact on the operation but to be consistent with the rest of the range we favor the Led down, and in this case, the flat cable is twisted.