Issue:
Wants to disable or ignore a CLI on an ATV61/71.
Product Line:
Altivar 71
Environment:
All
Cause:
Drive is reaching CLI
Resolution:
CLI means current limit. It cannot be disabled or set to 'ignore'.
This is a drive state not a fault. It is there to protect your motor. If the drive stays in CLI for longer than one minute, it will fault on overload.
Wants to disable or ignore a CLI on an ATV61/71.
Product Line:
Altivar 71
Environment:
All
Cause:
Drive is reaching CLI
Resolution:
CLI means current limit. It cannot be disabled or set to 'ignore'.
This is a drive state not a fault. It is there to protect your motor. If the drive stays in CLI for longer than one minute, it will fault on overload.
Released for:Schneider Electric Nigeria
Issue:
Wants to disable or ignore a CLI on an ATV61/71.
Product Line:
Altivar 71
Environment:
All
Cause:
Drive is reaching CLI
Resolution:
CLI means current limit. It cannot be disabled or set to 'ignore'.
This is a drive state not a fault. It is there to protect your motor. If the drive stays in CLI for longer than one minute, it will fault on overload.
Wants to disable or ignore a CLI on an ATV61/71.
Product Line:
Altivar 71
Environment:
All
Cause:
Drive is reaching CLI
Resolution:
CLI means current limit. It cannot be disabled or set to 'ignore'.
This is a drive state not a fault. It is there to protect your motor. If the drive stays in CLI for longer than one minute, it will fault on overload.
Released for:Schneider Electric Nigeria