Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the M340 processor come with a SD card?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Issue:
Does the SD card come with the M340 Processor.

Product line:
All M340 processors

Environment:
EcoStruxure Control Expert

Resolution:
Yes, the BMXRMS008MP card is supplied with each processor