How can we help you today?

EcoStruxure Process Expert: How to use Runtime Navigation Services(RTNS)

Goals and Symptoms:

This Video explains the Feature Runtime Navigation Services(RTNS) available in Ecostruxure Process Expert

Facts and Changes:

This Video can be referred for any Ecostruxure Process Expert version

Causes and Fixes:

A service which helps the user to view the Instance-Related Information, such as system-based and/or user-based data for monitoring and troubleshooting purposes.
RTNS enables you to view:
The section of the control project that contains the components of the instance for which you want to view information.
The controller and Hardware information.
The instance or system related documentation.
Linked instances and their details.
Information on the controllers and station nodes to which the project is deployed.