Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to make the print_char work in character mode on both ports of BMXNOM0200?

1.Issue

Once customer enables the print_char block to one port of BMXNOM0200 with character mode(without connection on this port),  the print_char on the other port will stop working after 30sec.

2.Environment

Issue only happens when NOM is on the  BMxCRA312xx drop.

3.Resolution

Set the ‘Immediate acknowledge bit’  of GEST variable to TRUE. Then, the NOM module will immediately answer to the input character request even if no character is available so that it will release the communication resources in time.(attached snapshot)

4.FAQ Applicable Conditions

FAQ also applies to input_byte or input_char when using character mode on both ports & one port
experiences communication time out.

Schneider Electric Nigeria

Attachment(s)
NOMmode.png [15.05 KB]