Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many push button operators can an enclosed ATV320 have?
Issue :
Adding push buttons to enclosed ATV320.

Product Line :
Altivar drive

Environment :
Enclosed ATV320

Resolution :
The enclosed ATV320 can accommodate up to 2 single or dual functions push buttons from XB4/XB5/XB7 family.