Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Nutanix AHV: Prioritized VMs with 0 second Startup Duration are powered on

Issue:
When a UPS critical event is cleared and PowerChute starts powering on VMs, any prioritized VMs with a 0 second Startup Duration are initially skipped and later powered on.

Product Line:
PowerChute Network Shutdown v4.3, v4.4

Environment:
PowerChute Network Shutdown configured with Nutanix Acropolis Hypervisor (AHV) support

Solution:
This issue will be resolved in the PowerChute Network Shutdown 5.x release.

Alternatively, if your PowerChute configuration includes priority groups with a 0 second Startup Duration, you can disable VM Startup in PowerChute and power on VMs manually following a shutdown.