Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to enable Product Restart via communication for Altivar ATV variable speed drives
There are 2 parameters for product restart.
One is RP. If value 1 is written to RP, the product will restart. In this way product restart can be activated via HMI as well. RP has logic address 16#1BD8 = 7128
Second method is to assign a logic input or a bit written via communication. Assignment can be done via HMI. Somove or communication. See attached table with the possible RPA assignment.
For example if you assign RPA= CD11, the product restart can be activated by bit 11 in CMD word sent by active control channel.

Schneider Electric Nigeria

Attachment(s)
RP, RPA.txt [4.01 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings