Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I program the ATV630 for +/- speeds via digital inputs?
Issue:
Programming reference switching and +/- speeds via digital inputs for the ATV630.

Product Line:
Process Drives

Environment:
ATV630  ATV930

Cause:
Setup +/- speed as second reference.

Resolution:
[Complete settings] [Command and Reference]
Freq Switch Assign =  Ref Freq Channel 2
Ref Freq 2 Config = Ref Frequency via DI

[Complete settings] [Generic functions] [+/- speed]
[+ Speed Assign] USP = desired DIx  Increase speed input assignment.
[- Speed Assign] dSP = desired DIx  Down speed input assignment.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings