Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In need of none or odd parity setting on the Link150 when Modbus ASCII is used

Issue:

The user may require a specific parity setting on the Link150 (EGX150) when the transmission mode has been set to Modbus ASCII

Product Line:

Link150 (EGX150)

Resolution:

When the transmission mode is set to Modbus ASCII, the parity of the serial port is limited to EVEN. Unfortunately, parity cannot be adjusted to none or odd.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings