How can we help you today?

How To convert DNP3 Variables from a BMXNOR0200 export file to an Array using the Unity Excel Tool

Issue
How To convert DNP3 Variables from an RTUConf file from a BMXNOR0200 to an Array using the Unity Excel Tool

Product Line
BMXNOR0200

Environment
Windows 7, Windows 10, Windows 8

Resolution
The purpose of this video is to demonstrate how to convert a group of DNP3
variables that have been configured in an BMXNOR0200 as single unlocated
variables, into an Unity unlocated variable array.   The DNP3 variables from the
NOR are converted using both an 'RTUConf' export file and the Unity Excel Tool.

The steps in this video will show the user how to:

1.) Import the 'RTUConfig.xml' file into an Excel spreadsheet,

2.) Extract the DNP3 variable name and type from the
spreadsheet and import into the Unity Excel Tool.

3.) Create a Unity Data Editor Variable '.xsy' export file.

4.) Import the '.xsy' file into Unity.

5.) Implement the new array variables in the BMXNOR0200

https://youtu.be/rowQJ3VzOeE?t=11

Schneider Electric Nigeria