Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the ATV12 capable of BACnet communication?
Issue:
Setting an ATV12 for BACnet communication

Product Line:
Altivar 12

Environment:
All

Cause:
Needing BACnet communication functionality

Resolution:
No, the ATV12 is not capable of BACnet communication.