{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SBO server communication on different TCP ports
Testing installation:
ES software administrator
HTTP: 80, HTTPS: 443, TCP: 5555
ES Workstation: Communication tab
ES <ip.addr.> TCP port 5555 <editable>
AS <ip.addr.> TCP port 4444 <editable>
AS Workstation: Communication tab
ES <ip.addr.> TCP port 5555 <editable>
AS <ip.addr.> TCP port 4444 <read only>

COMMUNICATION:
Type 1
Enterprise server                                                  AS-P
58563 <--------------------- PSH ACK ------------------------ 4444
58563 ---------------------- PSH ACK -----------------------> 4444
58563 <---------------------    ACK     ------------------------ 4444
58563 ----------------------     ACK     -----------------------> 4444
Type 2
Enterprise server                                                  AS-P
5555 <--------------------- PSH ACK ------------------------ 54465
5555 ---------------------- PSH ACK -----------------------> 54465
5555 <---------------------    ACK     ------------------------ 54465
5555 ----------------------     ACK     -----------------------> 54465

Both type are used during communication.
It depends on type of information which is transfered.

Schneider Electric Nigeria