Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can an Ethernet module be added to a "Non-E" version of an ATV340 series drive?
Issue:
Customer has purchased a "non-E" version of the ATV340 drive but needs to communicate with the drive via Ethernet.

Product Line:
Altivar Machines, Altivar 340

Environment:
"Non-E" version of the drive (last digit of part number is NOT an E)

Cause:
Clarification of product capabilities.

Resolution:
No. An ATV340 drive that does not have integrate Ethernet communication options can not have them added via an option card.   There are two versions of the ATV340 series drive, the E and the Non-E.  If Ethernet communication is needed you must purchase the E version (Last digit of part number is E).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings