Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the AR9000RAMP reusable? If so, how many times can it be reused?
Issue:
There is no documentation stating how many times the ramp can be reused.

Product Line:
NetShelter SX HS

Environment:
All versions and serial ranges.

Cause:
It is unknown whether the AR9000RAMP is reusable.

Resolution:

Yes, the AR9000RAMP is reusable.
Although there is no set number of times it may be reused, the Installation Manual has the following statement: