{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PSO (Power SCADA Operation) IO Server crashes while communicating on ION protocol with ION meters.

This is because the current driver driver does not handle frameworks with gaps in recorders properly. To fix the issue we have following workaround. Please correct template of all ION meters as follows using latest ION Setup.

  • Open Advanced Configuration Mode for the meter to be edited
  • Navigate to Data Rec Module > EgyDmd
  • The Energy Demand log is configured to use Sources 8,9,10, As by default it uses Sources 1,2,3
  • Edit the Inputs and change the Inputs to use Sources 1,2 and 3.
  • This must be done for all ION meters communicating to PSO over ION protocol
  • See attached PDF for detailed description for the same.

Schneider Electric Nigeria

Attachment(s)
IO Server crashes while communicating on ION protocol with ION meters.pdf [116.8 KB]