Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What connections types are accepted on ATV340 for encoder usage?
Issue:
Connections types accepted on ATV340 for encoder use.

Product Line:
Altivar 340

Environment:
All

Cause:
Connection type

Resolution:
ATV340  has an embedded encoder input (socket CN3) of standard: D-sub 15HD
Optional encoder cards for ATV340:
VW3A3420        -    D-sub 15HD
VW3A3423        -    D-sub 9
VW3A3422        -    D-sub 15HD